SIMATIC NET
SINEMA E Version 2006 + SP4 + HF1 (simply referred to
as SINEMA E below)
Installation and User Instructions
These instructions can be considered more valid than
contradictory statements made in other documents.
Please read these instructions carefully. They contain
important information on installing and using SINEMA E.
Important
hints for the usage of SINEMA E
Area of application of SINEMA E
SINEMA E is a PC software package for
planning, commissioning and servicing WLAN networks according to the IEEE
802.11 a/b/g/h standards.
SINEMA E includes functions for
simulation, measurement (site survey) and configuration of SCALANCE W clients and access points and
documentation of the results.
Experience
with WLANs is essential to be able to work correctly with SINEMA E and to interpret the results.
Planning and reality
The
planning accuracy is largely dependent on the accuracy with which the
environment is modeled. During the planning phase with SINEMA E, complete and precise modeling
of the environment is not always possible either because the environment only
exists in plans or because full modeling would involve too much effort. For
this reason, if the environment cannot be captured completely, it is sometimes
more practical to use SINEMA E
for planning WLANs based simply on the obstacles available from the catalog.
This procedure can turn out to be a good compromise between simulation accuracy
and the effort involved in modeling.
Although
the materials and regions available in the catalog are based on measurements
made in existing environments, the properties used, such as attenuation,
environmental conditions etc. may nevertheless differ from the actual materials
and regions depending on the environment. The simulation results may therefore
differ to a greater or lesser extent. Whenever possible, simulation accuracy
should be increased by measuring each region and each material used with SINEMA E before you model the
environment.
SINEMA E is particularly suitable for
indoor applications and outdoor applications in the immediate vicinity of
buildings. SINEMA E was not,
however, designed for purely outdoor applications over larger distances, such
as directional wireless links, and was not released for such applications.
Planning
and simulation results must always be verified by local RF field measurements.
Differences between planning and reality can be recognized best in the SINEMA E differential view and
deviations minimized by optimization (modifying device parameters and changing
the position of antennas etc.).
Differences
between planning and reality may be result for the following reasons:
·
Inaccurate
modeling of the environment by the user
·
Measurement
errors
-
due
to component tolerances of the WLAN map used for the measurement
-
due
to user error
·
Temporary
or environmentally-related fluctuations in the RF field due to
-
other active transmitters in the WLAN frequency
range (microwave, Bluetooth etc.)
-
persons
and moving objects (for example empty, half full or full storage bays)
-
Dust,
fog and rain
Configuration
The
configuration of the SCALANCE W
access points and clients supports multiple device parameter settings required
for the basic commissioning of the WLAN network. Web-based management can be
called up for special parameter settings.
Which environments are excluded?
The use
of SINEMA E is excluded for the
following environments and applications.
·
Outdoor
applications over longer distances, such as directional wireless links
·
All
applications in environments categorized as being dangerous to life or liable
to cause injury, such as nuclear plants, traffic management systems for
aircraft, railways and automobiles, extremely dusty environments; mines
Otherwise, the conditions of the sales
agreement apply.
Contents
1 Components of the
Product
1.1 New features in
SINEMA E 2006 SP3
1.2 New features in
SINEMA E 2006 SP4
2 Hardware
Requirements
3 Software
Requirements
3.1 Environment for Running the Program
3.2 Hard Disk Requirements
4 Installation
Instructions
4.1 Installing SINEMA E
4.2 License Key for SINEMA E
4.3 Uninstalling SINEMA E
4.4 Install shied error messages
4.5 Internet setup
5 Further Notes
5.1 Event Settings for Access Point Version 2.3.5
5.2 STEP 7 Function "Edit Ethernet Node" or Use of
the Primary Setup Tool not Possible
5.3 Unencrypted Password Transfer
5.4 Long Load Times for Wireless Upload/Download with Clients
5.5 Settings for Communication over Routers
5.6 Catalog & Properties
5.7 Do Not Modify Files
5.8 Do Not Use Bluetooth Adapters
5.9 FAQ on project engineering and configuration
5.10 iPCF (client SCALANCE W747-1RR)
5.11 Example project
5.12 Report
5.13 Noise Level and SNR Measurement with different WLAN cards
5.15 Site survey advanced mode - restrictions
5.16 Cross exchange of two IP-addresses
5.17 Exchange of SINEMA E projects
5.18 DPI configuration of the Graphical adapters
5.19 Supported site survey WLAN adapter
5.20 Supported site survey WLAN Adapter for advanced mode
5.21 Update of SINEMA E
2006 Lean / SINEMA E 2006 SP1 to SINEMA E 2006 SP2
5.22 Measuring with the material builder
5.23 Important information on difference view
5.24 Router address = IP-address
5.25 Dependency between site survey settings and calculation time
for site survey graphs
5.26 Supported channels in advanced site survey mode
5.27 SINEMA E advanced mode driver not installable
5.28 Site survey measurement in Standard Mode
5.29 Import of foreign antenna pattern
5.30 Site survey measurement of 802.11h networks
5.31 How to choose site survey adapter for region and material
builder in SINEMA E Lean version
5.32 Speed up auto-placement / reduce memory allocation
5.33 Data rates when channels overlap completely
5.34 Supported characters in DHCP client ID
5.35 Site survey driver for
5.36 Continuous mode indicates a much weaker signal strength value
than standard mode
5.37 Bird’s eye view window
5.38 Standard mode
5.39 Advanced mode
5.40 Adding Wi-Fi Protected Access Version 2 (WPA2) support to
Microsoft Windows XP SP2
5.41 Advanced Mode driver does not support the simultaneous use of
multiple Atheros-based Adapters
5.42 Enable SNMP v3
5.43 Troubleshooting
5.44 Relation between resolution of simulation and duration of
simulation
5.45 Limitations when using Auto placement
5.46 Lock channel, lock power
5.47 Opening in ceiling
5.48 Jump to location & access points out of the view area
5.49 Released antennas for access points
5.50 New hardware revisions of SCALANCE W devices
5.51 SINEMA E crashes while opening IWLAN PB Link Client
Properties page in Tablet PC
5.52 Released list of SCALANCE devices
5.53 SINEMA E Version 2006 SP1 or SINEMA E Version 2006 SP2 should
not be installed over later versions (starting at SP3)
5.54 SINEMA E Version 2006 SP3 (and following versions) setup
installs Site Survey Driver silently
5.55 Re-installing Site Survey Driver Setup since SINEMA E 2006
SP3
5.56 How to change “region domain code” of Advanced Mode Driver
5.57 SINEMA E Site Survey:
It is not possible to capture 184,188 (
5.58 In the current SINEMA E version the
following devices will be using “Alpha Networks wireless card with Atheros
chipset” Country certification instead of “siemens wireless card“ country
certification.
5.59 Load to SINEMA: Assigning online device
to project devices.
5.60 Information regarding Country
certification for Scalance W devices
5.61 SINEMA E Site Survey: Create User
Defined Data Record
5.62 Using Remote Desktop for operating SINEMA E
5.63 Information regarding Firmware Update feature
5.64 TIA – Totally Integrated Automation
5.65 Change of the deployment country
1 Components of the Product
This CD contains a complete SINEMA E installation in
two languages. Please read the section "Software Requirements" for
information on supported operating systems.
SINEMA E 2006 Lean license - Order number: 6GK1781-0AA00-6AA0
SINEMA E 2006 Standard license - Order number: 6GK1782-0AA00-6AA0
SINEMA E 2006 Power Pack for Standard License - Order number: 6GK1782-4AA00-6AC0
The corresponding functionality is activated by key
disk.
This package contains the following components:
· 1 SINEMA E CD
· 1 SIMATIC NET
Manual Collection CD
· 1 USB Stick with
license key
· 1 Certificate of
License
Content of the SINEMA E CD
·
SINEMA
E Version 2006 SP4
·
Notes
on the product "readme.htm"
·
"Configuration
Manual"
·
"Getting
Started" manual
·
Automation
License Manager
·
.net
Framework
·
site
survey driver
After completing the installation the manuals are
available on your computer by Start – Simatic – Documentation
1.1 New
features in SINEMA E 2006 SP3
·
New Advanced Mode Driver is based on Atheros driver
version: 5.3.0.56
·
New
Advanced Mode Driver solves WPA2 (Wi-Fi Protected Access version 2) security
settings issue
·
New Advanced Mode driver is compatible with all cards
with the following Atheros chipsets:
AR5001A,
AR5001X, AR5001X+, AR5002X, AR5002G, AR5004G, AR5004X,
AR5005G, AR5005GS, AR5006X, AR5006G, AR5006GS, AR5006XS, AR5006EXS,
AR5006EX, AR5006EGS, AR5006EG, AR5007G,
AR5007EG
1.2 New
features in SINEMA E 2006 SP4
·
Trending Graph
·
Firmware Update
2 Hardware
Requirements
To work with SINEMA E, you require a programming
device or
a PC that meets the following minimum requirements in
terms of processor speed, memory and graphics:
Processor RAM Graphics
----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
1Ghz 512 MB * XGA 1024x768 16-bit color depth
* A main memory of at
least 1024 MB is recommended.
For optimum display of the information, you should set
the colors in the Control Panel of your PG/PC to at least 65535 colors.
3 Software
Requirements
3.1 Environment
for Running the Program
Operating Systems
SINEMA E is a 32-bit application that can be run with
the following operating system:
Operating System Service
Pack
----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
MS Windows XP Professional SP3
MS Windows
You will find more detailed information on the
Microsoft Web site.
Internet Explorer
The MS Internet Explorer 6.0 is required with all
operating systems.
User Permissions
You can work with SINEMA E under MS Windows if you are
logged on with user permissions.
To install the software, you require administrator
privileges.
Acrobat Reader
To open the PDF documents on the CD, you require the
Acrobat Reader V4.0 or higher.
3.2 Hard
Disk Requirements
SINEMA E Hard Disk Requirements
SINEMA E requires approx. 45 MB of space on
your hard disk. The exact space also depends on your operating system and the
file system you are using on your PG/PC.
4 Installation
Instructions
The installation instructions contain important
information that you require to install SINEMA E. Please read the instructions before
you start the installation.
4.1 Installing
SINEMA E
Insert the installation CD in the drive. The program
is installed by a menu-guided setup.
The installation program starts automatically after
you insert the installation CD. If you have disabled this function on your
computer, start the setup program with the MS Windows Explorer by
double-clicking on the SETUP.EXE program in the root directory of your CD.
Follow the instructions of the setup program.
Hint: When the “My Documents” folder is located on a
network device that is currently not available SINEMA E is not installable. To
solve this problem:
·
Remount the device or
·
Change the “My Documents” path to an available path
temporary by changing the following registry entry.
[HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\Shell
Folders]
"Personal"="\\\\erld250a.ww004.siemens.net\\Home48$\\km3805\\My
Documents"
4.2 License
Key for SINEMA E
Before you can work with SINEMA E, you have to transfer
the license key (user authorization) from the license key disk to the computer.
The license can be transferred during the setup.
During installation of SINEMA E a dialog titled
“Automation License Manager” will be opened. The “Automation License Manager”
window must be set to front if it not shown in foreground and Transfer the
license in this dialog from floppy disc to your hard drive. After license
transfer or a SINEMA E license is already installed, close the dialog and the
installation will proceed.
If you have not transferred the license during setup,
restart your computer and transfer the key using the Automation License
Manager. You start this with the Start menu entry SIMATIC\License
Management\Automation License Manager. Insert the diskette in your floppy drive
and transfer the license key to your local hard disk. You can also transfer the
license key from the license key disk to a USB stick and transfer it from there
to the local hard disk.
---------------------------------------------------------------------------------------------------------------------------------------------------
Note
The Automation License Manager prevents the
installation of authorizations and license keys to invalid drives or media such
as RAM drives, diskettes or compressed drives (for example DBLSPACE). If the
hard disk of the device is registered as "removable disk" with a hard
drive mobile rack, it will be treated not as usual as a "hard disk"
but as a CD which means that no license keys can be installed on it.
If you have compressed drives, you can install the
license on the host drive.
Make sure that you follow the instructions in the
README.WRI file of the Automation License Manager on the installation CD in
"Automation License Manager\disk1\".
The folder "<drive on which the
authorization/license key is installed>:\AX NF ZZ" contains hidden
files. Do not under any circumstances delete, move or copy these files or the
folder. They contain data required for licensing your software!
If you ignore this warning, you take the risk of
losing your authorization/license key irrevocably.
---------------------------------------------------------------------------------------------------------------------------------------------------
Notes on Correct Use of the License Key:
· The license key diskette must not be read-only. Since the license key
diskette is used without write protection, there is a risk that a virus could
be transferred from the hard disk to the diskette. Whenever you install or uninstall
a license key, you should therefore first scan your PG / PC for viruses.
· If you use an optimizing program that provides the option of moving
fixed blocks of data, only use this option once you have transferred the
license key from the hard disk back to the license key diskette.
· When you install the license key, a special cluster is created on the
destination drive. Some checking programs show this cluster as being
"defective". Do not try to repair this cluster.
· Before you format, compress or restore your hard disk and before you
install a new operating system, remember to transfer the license key back to
the license key diskette.
· If a backup copy of your hard disk contains copies of license keys,
there is a danger that these copies may overwrite and destroy still valid
license keys if you restore your backup data to the hard disk. To prevent a
valid license key being overwritten by a backup copy, we strongly recommend
that you either remove all license keys before you make a backup copy or that
you exclude the license keys from the backup.
Using the Trial License
If no
valid license key is installed for SINEMA E, a trial license key is used that
is supplied and installed as standard with SINEMA E. SINEMA E can, however,
only be used for 14 days with this license key. The trial license is activated
the first time you start SINEMA E without a valid license key.
4.3 Uninstalling
SINEMA E
Uninstalling software products must conform to the
procedures in MS Windows.
To uninstall your software package (for example
"SINEMA E Version 2006 SP2") use the MS Windows application
"Add/Remove Programs" (MS Windows taskbar with Start > Settings
> Control Panel > Add/Remove Programs).
As an alternative, you can use the setup program to
uninstall the package.
NOTE: Please do not
uninstall Sinema E Version 2006 + SP1
using Microsoft Windows “Add/Remove Programs” application.
4.4 Install
shield error messages
When Install shield error messages occur during the
installation process, so search for the error description and help by using the
error number.
·
Start your web browser and open the page www.google.com
·
Type in following search string “install shield + error
number + site” in e.g. “install shield + 1607 + site”.
4.5 Internet
setup
Please pay attention to the following installation
order for the Internet setup
1.
Microsoft Visual C++ 2005 Redistributable Package
The Microsoft Visual C++ 2005 Redistributable Package can be downloaded
following this link
http://www.microsoft.com/downloads/details.aspx?displaylang=en&FamilyID=32bc1bee-a3f9-4c13-9c99-220b62a191ee
2.
.Net Framework 2.0
The .Net Framework 2.0 can be downloaded
following this link
http://www.microsoft.com/downloads/details.aspx?FamilyID=0856EACB-4362-4B0D-8EDD-AAB15C5E04F5&displaylang=en
3.
Automation License Manager
4.
SINEMA E + Driver
5 Further
Notes
5.1 Event
Settings for Access Point Version 2.3.5
Setting the event "Force Roaming on IP
down" in access point firmware version 2.3.5 returns an error.
Solution
· With firmware version 2.3.5
o
Disable
the setting "Force Roaming on IP down" in SINEMA E in the Parameter
Editor in the Events category
o
Load
the configuration to the access point with "Load to Device"
o
Enable
the option using Web based Management.
· As an alternative to the solution mentioned above, you can also replace firmware version 2.3.5 with firmware version 2.4. This problem no longer occurs in this firmware version.
o
You
will find new firmware versions by clicking on the following link
5.2 STEP 7 Function “Edit Ethernet Node” or Use
of the Primary Setup Tool not Possible
When SINEMA E has been started, it is not
possible to work with STEP 7 function “Edit Ethernet node” and Primary Setup
Tool.
Solution: Exit SINEMA E before you use STEP 7 or the
Primary Setup Tool.
5.3 Unencrypted
Password Transfer
With the following online function, SINEMA E
transfers an unencrypted password. (Only firmware version 2.3 / 2.4)
· Load to SINEMA
· Load to Device
· Backup
· Reset
5.4 Long Load Times for Wireless
Upload/Download with Clients
With SINEMA E, the load times with clients of
the type SCALANCE 74X can be longer than normal, if the clients have a firmware
version lower than 3.0.
5.5 Settings for Communication
over Routers
To be able to communicate over a router between
the engineering system and wireless devices, both ends (engineering system and
the destination system) must have the router entered as default gateway. The
router must therefore allow access over both networks and the Telnet/TFTP ports
must be enabled on the router.
5.6 Catalog & Properties
If you have modified entries in the global
library, you can synchronize these with the project catalog.
Notice: The number of interfaces of the access points
is not synchronized!
The modifications are displayed in the 'Catalog
& Properties' window only after the synchronized object has been selected
again.
5.7 Do Not Modify Files
Notice: Do not modify any files installed by SINEMA E!
· Project files
· Catalog files
· Configuration files
If you modify files, it will not be possible to
run SINEMA E free of errors or you will not be able to open existing projects.
5.8 Do Not Use Bluetooth
Adapters
With SINEMA E do not use Bluetooth adapters
displayed in 'Options > Network adapters'!
SINEMA E is not designed for this and you may
otherwise encounter problems in the running of the program.
5.9 FAQ on project engineering
and configuration
In the Configuration Manual in chapter 5.1.5
under the entry ‘How can I enable or disable SINEMA E as an exception for the
Windows XP Firewall?’ you can find the notice that SINEMA E uses while loading
the configuration the ports TFTP (default port number 69) and Telnet (default
port number 23).
5.10 iPCF (client SCALANCE W747-1RR)
iPCF is only possible, if the option
‘Connect to any SSID’ is disabled.
5.11 Example project
Example project file for SINEMA E can be found
in the folder “Example” in the installation path. The example project can be
opened in SINEMA E in the help menu.
5.12 Report
The antennas, which are placed by
the Sales Wizard, display in the table ‘Access Point Information’ the x-position 0 and the y-position 0.
You can get the right position of
the antenna from the x-y-position of the access point.
5.13 Noise Level and SNR Measurement with different
WLAN cards
The Noise level and the dependent
SNR value are strongly dependent on different WLAN adapter cards. This is
caused by the different WLAN cards.
5.15 Site survey advanced mode - restrictions
The advanced mode was tested under
German country regulations.
5.16 Cross exchange of two IP addresses
If two devices with the same IP
address exists in a real network and the user want to exchange the IP address,
please follow the following instructions
·
Start
the Online Function “initial setup”.
·
Change
the IP address of the first device to a free IP address.
·
Load
all devices by using the online function “Load to device”.
5.17 Exchange of SINEMA E projects
To save disk space while exchanging
SINEMA E projects – use “Save copy of project as ...” functionality. This
function saves only the necessary files for project exchange.
5.18 DPI configuration of the Graphical adapters
For a correct presentation use 96
dpi for the display settings. The configuration is reachable by right mouse
button menu while pointing to the desktop – properties – tab settings –
advanced settings – tab general.
5.19 Supported site survey WLAN adapter
MS Windows XP SP2:
Following WLAN adapters are
supported by “SINEMA E advanced mode” driver in advanced and standard mode.
·
SIMATIC
NET CP 7515
·
D-Link
Air Premier DWL-AG660 FW 2.30
·
Cisco
Aironet CB21AG-E-K9
·
Proxim
ORiNOCO 802.11a/b/g ComboCard 8480-FC
·
Netgear
Dual Band Wireless PC Card WAG511 v2
Following WLAN adapters are not
compatible with the SINEMA E advanced mode driver and can not be used in
advanced mode.
·
D-Link
AirXpert DWL-AG650/660 Wireless Cardbus Adapter (A/B/G)
Hint: Standard
mode works with all WLAN adapters that are supported by Windows.
MS Windows
All WLAN adapters that are supported
by Windows Vista are also supported by SINEMA E.
The following WLAN adapters are
recommended:
·
SIMATIC
NET CP 7515
·
D-Link
Air Premier DWL-AG660 FW 2.30
·
Cisco
Aironet CB21AG-E-K9
·
Proxim
ORiNOCO 802.11a/b/g ComboCard 8480-FC
·
Netgear
Dual Band Wireless PC Card WAG511 v2
·
Intel
Pro/Wireless 3945ABG network adapter
·
D-Link
USB-Adapter DWL-122
5.20 Supported site survey WLAN Adapter for
advanced mode
MS Windows XP SP2:
For the advanced site survey mode
the “Advanced mode driver” is needed.
The driver is based on the Atheros V
5.3.0.56 wireless driver.
The driver is compatible to all
cards based on the following Atheros chipset:
AR5001A, AR5001X,
AR5001X+, AR5002X, AR5002G, AR5004G, AR5004X,
AR5005G, AR5005GS, AR5006X, AR5006G, AR5006GS, AR5006XS,
AR5006EXS,
AR5006EX,
AR5006EGS, AR5006EG, AR5007G, AR5007EG
How can I tell what chipset my wireless adapter
is using?
What wireless adapters are commercially
available those are using these chipsets?
View http://customerproducts.atheros.com/customerproducts/ResultsPageBasic.asp
to find out.
The number of commercially available
wireless adapters using these chipsets is quite large. SIEMENS has tested a
representative sample of these adapters to validate our driver’s support for
these chipset families.
·
SIMATIC
NET CP 7515
·
D-Link
Air Premier DWL-AG660 FW 2.30
·
Cisco
Aironet CB21AG-E-K9
·
Proxim
ORiNOCO 802.11a/b/g ComboCard 8480-FC
·
Netgear
Dual Band Wireless PC Card WAG511 v2
MS Windows
All WLAN adapters that are supported
by Windows Vista are also supported by SINEMA E.
The following WLAN adapters are recommended:
·
SIMATIC
NET CP 7515
·
D-Link
Air Premier DWL-AG660 FW 2.30
·
Cisco
Aironet CB21AG-E-K9
·
Proxim
ORiNOCO 802.11a/b/g ComboCard 8480-FC
·
Netgear
Dual Band Wireless PC Card WAG511 v2
·
Intel
Pro/Wireless 3945ABG network adapter
·
D-Link
USB-Adapter DWL-122
5.21 Update of SINEMA E 2006 Lean / SINEMA E 2006
SP1 to SINEMA E 2006 SP2
If the user installs SINEMA E 2006
SP2 over an existing previous version a rollback to the previous version is
only possible by uninstalling and reinstall of the previous version.
Upgrade from Windows XP to Windows
Please follow these steps:
·
Transfer
the SINEMA licence key to the key disc or an usb device
·
Uninstall
SINEMA E from the Windows XP system
·
Do
upgrade from Windows XP to Windows Vista
·
Install
SINEMA E 2006 SP2
5.22 Measuring with the material builder
To measure a new obstacle use the
obstacle type “undefined obstacle” and the obstacle tool “normal”.
5.23 Important information on difference view
The mapping between a measured value
and a simulated value is done by checking on the same BSSID and SSID. If the
user does not define a BSSID in the project the mapping can not be done. So
please define a BSSID in the project for the access points that should be
compared in difference view.
5.24 Router address = IP address
In Web based management
of the SCALANCE-W router-address can be set to the same value as the
ip-address.
It is not possible to do
the same using the SINEMA E online functions. The router-address is not set.
In an existing IP-Configuration
of an online device with IP-address = router-address, the router-address is
lost. The problem will be fixed with a new firmware version.
5.25 Dependency between site survey settings and
calculation time for site survey graphs
Following settings have
an influence in the calculation time / performance for site survey graphs.
·
Floor
size ( calibration )
·
Coverage
Map Profile
For best performance
·
Use
small floor sizes
·
Use
“Min” profile
5.26 Supported channels in advanced site survey
mode
Following channels are supported in
advanced mode.
802.11a
channel
36 | 5180 MHz
channel
40 | 5200 MHz
channel
44 | 5220 MHz
channel
48 | 5240 MHz
channel
52 | 5260 MHz
channel
56 | 5280 MHz
channel
60 | 5300 MHz
channel
64 | 5320 MHz
802.11h
channel
36 | 5180 MHz
channel
40 | 5200 MHz
channel
44 | 5220 MHz
channel
48 | 5240 MHz
channel
52 | 5260 MHz
channel
56 | 5280 MHz
channel
60 | 5300 MHz
channel
64 | 5320 MHz
channel
100 | 5500 MHz
channel
104 | 5520 MHz
channel
108 | 5540 MHz
channel
112 | 5560 MHz
channel
116 | 5580 MHz
channel
120 | 5600 MHz
channel
124 | 5620 MHz
channel
128 | 5640 MHz
channel
132 | 5660 MHz
channel
136 | 5680 MHz
channel
140 | 5700 MHz
802.11b/g
channel
1 / 2412 MHz
channel
2 | 2417 MHz
channel
3 | 2422 MHz
channel
4 | 2427 MHz
channel
5 | 2432 MHz
channel
6 | 2437 MHz
channel
7 | 2442 MHz
channel
8 | 2447 MHz
channel
9 | 2452 MHz
channel
10 | 2457 MHz
channel
11 | 2462 MHz
channel
12 | 2467 MHz
channel
13 | 2472 MHz
5.27 SINEMA E advanced mode driver not installable
Please make sure that the network
card is plugged while installing the driver.
5.28 Site survey measurement in Standard Mode
When several access points exists in
a plant with the same SSID, only the signal level of the AP will be measured
where the PC is logged in. When the signal level of the other access points
should be measured, please logout and login to the other access points and
measure again.
5.29 Import of foreign antenna pattern
To import antenna pattern of a foreign
format you can use the import functionality included in the antenna pattern
dialog.
File format description:
The import file is CSV.
·
The
values are row oriented.
·
The
values are separated by comma or semicolon
·
Only
“.” Not “,” for decimal places supported.
·
Phase
is from -180° to + 180°
·
Attenuation
is in db
Example:
* mode
patternmode=horizontal;
* for fine adjustment of the phase
phaseadjustment=90;
* is the phase inverted compared to SINEMA E
phasefactor=-1;
* attenuation of SINEMA E center point
attenuation_centerp=-60
* phase;attenuation
-179.000;-40.847
-178.000;-43.709
………;
179.000;-40.529
180.000;-39.759
Keyword description
|
Keyword |
Comment |
example |
|
* |
Leads in a comment |
* this is a comment |
|
phaseadjustment |
In many
cases the phase the vendor uses another orientation for the 0° angle. Use
this attribute to adjust. The parameter should work in the SINEMA E GUI
logic. -180° … 180°
|
Phaseadjustment=90
|
|
Phasefactor |
Some vendors
inverted the angle logic. |
Phasefactor
= -1 …to invert the angle |
|
Patternmode |
Specifies
whether it is a horizontal or a vertical pattern horizontal = horizontal pattern vertical = vertical pattern |
patternmode=horizontal patternmode=vertical |
|
attenuation_centerp |
Attenuation
in the center of the pattern |
attenuation_centerp=-60 |
5.30 site
survey measurement of 802.11h networks
The mode of site survey measurements
of an 802.11h networks is shown as 802.11a or g mode.
5.31 How to choose site survey adapter for region
and material builder in SINEMA E Lean version
The network adapter can be selected
in (Start \ Setting \ Control Panel \ network connections \ wireless network
connections).
When more than one is activated, the
first activated is used. The actual used network adapter is shown in the
statistic of the measurements.
5.32 Speed up auto placement / reduce memory
allocation
To speed up the auto placement
algorithm and minimize memory allocation the checkbox “channel optimization
after auto placement” can be unchecked. Uncheck this option, when SINEMA E
announces too less memory.
5.33 Data rates when channels overlap completely
If channels of access points are overlapping
completely the predicted data rate viewed in SINEMA E is too pessimistic.
You can estimate the correct data
rate at a point by using the maximum data rate of the overlapping access points
at this point and divide it through the amount of access points at this point.
e.g.
2 overlapping AP
Both can reach 54 Mbit/s at the
point
Resulting data rate = 24Mbit/s
5.34 Supported characters in DHCP client ID
Only characters of the international
ASCII character set are supported for client ID of DHCP.
5.35 Site survey driver for
Microsoft Windows Vista and higher
versions provide built-in support for 802.11 Wireless LAN networking. So, site
survey driver is not required.
5.36 Continuous mode indicates a much weaker signal strength value than
standard mode
Continuous mode records measurements
between START and END point defined by the user. These measurements are mapped
to floor plan map based on measurement grid size value and number of
measurements recorded within each grid. Since we are calculating MEAN value of
measurements within each grid, signal strength value of continuous mode may
slightly vary with standard mode values.
5.37 Bird’s
eye view window
To improve
zoom functionality and to show the “user interested area” easily, the ‘Bird’s
eye view’ window is added into the project navigator. The user can view
complete “view area” in a small feed back window and he can easily navigate in
the main window.
You can open
and close the ‘Bird’s eye view’ window with the “Show Bird’s Eye” view tool bar button in the tool bar of the
modeling editor.
Functions
of Bird’s eye view:
·
Select view area: The user is able to define his
view area, depending on user selected area in Birds eye view. The main window
is zoomed and scroll bars are set such that user selected area is exactly being
fit to view window.
·
Show in actual proportion/stretched
view: The user is
able to choose if Bird’s eye view window should be proportional to the main
window or not.
Note: The
Bird’s eye view and the 3d view aren’t being refreshed for the selected window
when you have 2 or more windows opened as multiple views.
5.38 Standard Mode
·
Standard Mode Driver Hints
The standard mode works with all WLAN
adapters supported by Microsoft Windows XP SP2. In Windows XP SP2 environment
the user should use the latest driver from the adapter’s vendor for recording
standard mode measurements of a WPA2 enabled wireless network.
·
WPA2 Hints
o
Install
the new Microsoft WPA2 (Wi-Fi Protected Access version 2) patch for Windows XP
SP2. This update provides support for Wi-Fi Protected Access 2 (WPA2).
You can find the download here: http://www.microsoft.com/downloads/details.aspx?amp;amp;amp;amp;amp;amp;amp;displaylang=en&familyid=662BB74D-E7C1-48D6-95EE-1459234F4483&displaylang=en
o
Make sure your access point firmware supports WPA2. If necessary update
the firmware.
5.39 Advanced Mode
The advanced
mode driver is required for recording advanced mode measurements in Site Survey.
This is a special driver required under Microsoft Windows XP SP2 and is
available with the installation CD of SINEMA E. This driver is developed based
on Atheros driver version: 3.1.2.47.
The advanced
Mode driver under Microsoft Windows XP SP2 cannot be used with WPA2 (Wi-Fi
Protected Access version 2) security settings.
In this case
the previously installed device driver should be used (see: How to roll back a
device driver) or the latest driver from the adapter vendor should be installed.
·
How to install Advanced Mode
Driver:
o Insert SINEMA E installation CD in the drive. The installation program starts automatically after you insert the installation CD. Follow the instructions of the setup program and select Site Survey driver setup from the list. This installs advanced mode driver for SINEMA E.
o
If SINEMA E is already installed in
the machine, start driver setup from C:\Program Files\SIEMENS\SINEMA
E\driver\Installation file\Setup.exe
Hint: Please
make sure that the PCMCIA-WLAN adapter with Atheros chipset released for SINEMA
E Advanced mode is plugged-in while installing the driver.
·
Advanced
mode driver is not WPA2 compatible in standard mode:
Advanced Mode driver is
not WPA2 compatible even in Standard Mode. The advanced mode driver does not
support WPA2 security settings. If the Access Points in the wireless network
are protected with WPA2 and the advanced mode driver is assigned to the WLAN
PCMCIA adapter then no wireless communication is possible between the PCMCIA
adapter and the wireless network. This is the case even if SINEMA E is not
active or if you are trying to operate SINEMA E in standard mode.
·
Advanced Mode driver does not
support the simultaneous use of multiple Atheros-based Adapters:
Atheros
doesn't support this usage. Since advanced mode driver is based on Atheros
driver version 3.1.2.47, it does not support simultaneous use of multiple
Atheros-based adapters.
Solution:
o
One of the Atheros-based cards would
need to be disabled for the other Atheros-based card to function.
Please go
through the below link:
http://windowshelp.microsoft.com/Windows/en-US/Help/ca2d0191-299e-4dc3-afab-df5862d460be1033.mspx
5.40 Adding
Wi-Fi Protected Access Version 2 (WPA2) support to Microsoft Windows XP SP2
·
Install
the new Microsoft WPA2 (Wi-Fi Protected Access version 2) patch for Windows XP
SP2. This update provides support for Wi-Fi Protected Access 2 (WPA2).
You can find the download here: http://www.microsoft.com/downloads/details.aspx?amp;amp;amp;amp;amp;amp;amp;displaylang=en&familyid=662BB74D-E7C1-48D6-95EE-1459234F4483&displaylang=en
·
Make
sure your access point firmware supports WPA2. If necessary update the
firmware.
5.41 Advanced Mode driver does not support the
simultaneous use of multiple Atheros-based Adapters
Atheros
doesn't support this usage. Since advanced mode driver is based on Atheros
driver version 5.3.0.56, it does not support simultaneous use of multiple
Atheros-based adapters.
Solution:
§
One of the Atheros-based cards would
need to be disabled for the other Atheros-based card to function.
Please go
through the below link:
http://windowshelp.microsoft.com/Windows/en-US/Help/ca2d0191-299e-4dc3-afab-df5862d460be1033.mspx
5.42 Enable
SNMP v3
This
option enables the
transfer of traps of SNMP version 3. This option does not depend upon SNMPv1/v2c.
5.43 Troubleshooting
o
For external adapters make sure USB or PCMCIA Wireless
LAN adapter is plugged-in.
o
For internal Wireless LAN adapters make sure that the
device is switched to ON.
o
Check under windows network settings that the Wireless
LAN adapter is not activated.
Open Network
Adapters by clicking Control Panel,
clicking Administrative Tools,
clicking Computer Management, and
then clicking Device Manager.
Right click a network adapter and select Properties menu. To see the details of
the network adapter driver, click Driver
tab and then click Driver Details...
button. This will show driver file details.
Please go through the below link:
http://windowshelp.microsoft.com/Windows/en-US/Help/ca2d0191-299e-4dc3-afab-df5862d460be1033.mspx
In case of any problems with a newly
installed device driver, the previously installed device driver can be re-used
by following the instructions in the below link.
Please
go through the below link:
http://www.microsoft.com/windowsxp/using/helpandsupport/learnmore/driverrollback.mspx
5.44 Relation between resolution of
simulation and duration of simulation
The more fine
the resolution the more accurate the simulation is done, but the more time is
needed for simulation.
5.45 Limitations when using Auto placement
The
results of the auto placement algorithm are simply a recommendation, but do not
necessarily always provide the best location and number of access points. You
can however change the access point type, antenna, power and location in order
to achieve the required coverage for your application. Please remember that the
auto placement algorithm always uses omni-directional antenna, but in certain
cases directional antennas may give a better result.
Please
note following limitations of auto placement:
·
In
some cases the auto placement algorithm will achieve coverage of less than
100%. This is often cause by the fact that there are sometimes an insufficient
number of channels available at the WLAN mode in use. To achieve a better
coverage you should use a WLAN mode that supports a higher number of channels.
These settings can be changed in the options dialog.
The WLAN modes, e.g. in
o 802.11a = 4
o 802.11b = 3
o 802.11g = 3
o
802.11h = 19 indoor
o
802.11h
= 11 outdoor
The number can vary depending on country
regulations.
·
It’s
recommended to combine multiple small client areas into one area in order to
simplify the auto placement.
Limitations using Auto
placement outdoors
·
When
a client area is covered completely by forbidden areas then no access point can
be placed.
In this case increase the client area to the same size as the forbidden areas
(location and size). Auto placement will place the access points as required.
Limitations using Auto placement
indoors
To
identify the boundaries of the algorithm a bounding polygon over all walls is
being calculated. All Elements (walls, client areas, access points…) which are
outside of the bounding polygon are not considered during auto placement and
channel optimization.
Following
examples shall help to explain the functioning of the algorithm
o
A
building with 2 floors. In the lower one there is one access points. In the
upper one there is one client area. Both floors are “connected” with a opening
in the ceiling of the first floor. Starting the auto placement for the upper
floor will not consider the access point located in the lower floor. The auto
placement algorithm will place one additional access point in the upper floor
for covering the client area.
o
Client
areas which are partly inside a bounding polygon will not be covered by one
hundred per cent by the auto placement algorithm. Any way the algorithm might
show a coverage of 100%, since the part of the client area which lies inside
the bounding polygon is completely covered.
5.46 Lock channel, lock power
The two
properties ‘lock channel’ and ‘lock power’ can be found in the properties
window of an access point and when set to true they do prevent the values
channel and power being changed by channel optimization.
5.47 Opening in ceiling
A floor opening
is used to model a hole in the ceiling, with it you can model a lobby or
similar.
5.48 Jump to location & access points out of the view area
The function
“jump To Location” will not show the selected access point if this one is
placed outside the view area. The user has to zoom out manually to see the
object.
5.49 Released
antennas for access points
In order to
see which antennas are released for which access point the user has to use the
following link and browse for the suitable access point’s description.
5.50 New hardware revisions of SCALANCE W devices
On hardware
revision of access points and clients with the names does not changes, a
numbering in SINEMA up/download is added in the style of #X (where X is a
consecutive number).
5.51 SINEMA
E crashes while opening IWLAN PB Link Client Properties page in Tablet PC
This problem
occurs because of an error in Tablet PC and not with SINEMA E.
Please go through the below link:
http://support.microsoft.com/kb/941975/en-us (An application stops responding
when you use a tablet pen to mark items or to drag items on a Windows XP Tablet
PC Edition-based computer)
http://support.microsoft.com/kb/827220/en-us (Programs May Function Erratically
or Close Unexpectedly on the Tablet PC)
5.52 Released
list of SCALANCE devices
Please go
through the below link:
http://www.siemens.com/simatic-net/ik-info
Here you will find information about SCALANCE
devices and all country regulation information.
5.53 SINEMA
E Version 2006 SP1 or SINEMA E Version 2006 SP2 should not be installed over
later versions (starting at SP3)
Earlier
versions of SINEMA E releases (SP1 and SP2) won’t check for higher versions of
SINEMA E build. This is a known bug with setup. If you install SP1 or SP2 over
later versions all latest assemblies and binaries will be replaced with older
ones. Also ‘Add/Remove Programs’ will show program entries in Control Panel of
SP1 or SP2 and later versions of SINEMA E. So please don’t install SP1 or SP2
setup over later versions of SINEMA E.
5.54 SINEMA
E Version 2006 SP3 (and following versions) setup installs Site Survey Driver
silently
Since SINEMA
E Version 2006 SP3 the setup installs Site Survey Driver silently. It
internally detects the type of platform (XP or
5.55 Re-installing
Site Survey Driver Setup since SINEMA E 2006 SP3
If Site Survey Driver is uninstalled using
‘Add/Remove Programs’ and user wants to reinstall it, please uninstall and
install SINEMA E using the setup from the installation CD. Since SINEMA E
Version 2006 SP3 the Site Survey Driver will be installed silently.
5.56 How
to change “region domain code” of Advanced Mode Driver
Advanced
Mode Driver scans channels based on the region domain code specified in the
registry. By default, region domain code depends upon
the language
of the target machine’s operating system. If operating system’s language is
‘ENGLISH’, ‘Region Domain’ will be ‘US’ and for ‘GERMAN’ language, ‘Region
Domain’ will be ‘DE’.
Later User
can change this region domain code in the registry. You can find the region
domain key under the following key:
HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Control\Class\{4D36E972-E325-11CE-BFC1-08002bE10318}\????.
‘????’
specifies a 4-digit number which represents a network adapter.
The {4D36E972-E325-11CE-BFC1-08002bE10318}
subkey represents the class of network devices supported by the system. This
subkey contains several 4-digit numbered subkeys, which represent particular
network adapters. These subkeys store data that applies only to that device.
ccode subkey under a particular network adapter
determines the region domain for that adapter. You can set ccode subkey value based on the values given in the ‘Code’ column
of the below table. After setting a specific region code, please restart the
system in order to effect those changes.
|
Region
Domain |
Code |
11g |
Turbo 11a |
Turbo 11g |
|
"NO_COUNTRY_SET" |
"NA" |
YES |
YES |
YES |
|
" |
" |
YES |
NO |
YES |
|
" |
"DZ" |
YES |
NO |
YES |
|
" |
"AR" |
YES |
NO |
NO |
|
" |
"AM" |
YES |
NO |
YES |
|
" |
"AU" |
YES |
YES |
YES |
|
" |
"AT" |
YES |
NO |
YES |
|
" |
"AZ" |
YES |
YES |
YES |
|
" |
"BH" |
YES |
NO |
YES |
|
" |
"BY" |
YES |
NO |
YES |
|
" |
"BE" |
YES |
NO |
YES |
|
" |
"BZ" |
YES |
YES |
YES |
|
"BOLVIA" |
"BO" |
YES |
YES |
YES |
|
" |
"BA" |
YES |
NO |
YES |
|
" |
"BR" |
NO |
NO |
NO |
|
" |
BN |
YES |
YES |
YES |
|
" |
"BG" |
YES |
NO |
YES |
|
" |
"CA" |
YES |
YES |
YES |
|
" |
"CL" |
YES |
YES |
YES |
|
" |
"CN" |
YES |
YES |
YES |
|
" |
"CO" |
YES |
NO |
YES |
|
" |
"CR" |
YES |
NO |
YES |
|
" |
"HR" |
YES |
NO |
YES |
|
" |
"CY" |
YES |
YES |
YES |
|
" |
"CZ" |
YES |
NO |
YES |
|
" |
"DK" |
YES |
NO |
YES |
|
" |
DO |
YES |
YES |
YES |
|
" |
"EC" |
NO |
NO |
NO |
|
" |
"EG" |
YES |
NO |
YES |
|
" |
"SV" |
YES |
NO |
YES |
|
" |
"EE" |
YES |
NO |
YES |
|
" |
"FI" |
YES |
NO |
YES |
|
" |
"FR" |
YES |
NO |
YES |
|
"FRANCE_RES" |
"F2" |
YES |
NO |
YES |
|
" |
"GE" |
YES |
YES |
YES |
|
" |
"DE" |
YES |
NO |
YES |
|
" |
"GR" |
YES |
NO |
YES |
|
" |
"GT" |
YES |
YES |
YES |
|
" |
"HN" |
YES |
NO |
YES |
|
" |
"HK" |
YES |
YES |
YES |
|
" |
"HU" |
YES |
NO |
YES |
|
" |
"IS" |
YES |
NO |
YES |
|
" |
"IN" |
YES |
NO |
YES |
|
" |
"ID" |
YES |
NO |
YES |
|
" |
"IR" |
YES |
YES |
YES |
|
" |
"IE" |
YES |
NO |
YES |
|
" |
"IL" |
YES |
NO |
YES |
|
" |
"IT" |
YES |
NO |
YES |
|
" |
"JM" |
YES |
NO |
YES |
|
" |
"JP" |
YES |
NO |
NO |
|
"JAPAN1" |
"J1" |
YES |
NO |
NO |
|
"JAPAN2" |
"J2" |
YES |
NO |
NO |
|
"JAPAN3" |
"J3" |
YES |
NO |
NO |
|
"JAPAN4" |
"J4" |
YES |
NO |
NO |
|
"JAPAN5" |
"J5" |
YES |
NO |
NO |
|
"JAPAN6" |
"J6" |
YES |
NO |
NO |
|
"JAPAN7" |
"J7" |
YES |
NO |
NO |
|
"JAPAN8" |
"J8" |
YES |
NO |
NO |
|
"JAPAN9" |
"J9" |
YES |
NO |
NO |
|
JAPAN10 |
"J10" |
YES |
NO |
NO |
|
JAPAN11 |
"J11" |
YES |
NO |
NO |
|
JAPAN12 |
"J12" |
YES |
NO |
NO |
|
JAPAN13 |
"J13" |
YES |
NO |
NO |
|
JAPAN14 |
"J14" |
YES |
NO |
NO |
|
JAPAN15 |
"J15" |
YES |
NO |
NO |
|
JAPAN16 |
"J16" |
YES |
NO |
NO |
|
JAPAN17 |
"J17" |
YES |
NO |
NO |
|
JAPAN18 |
"J18" |
YES |
NO |
NO |
|
JAPAN19 |
"J19" |
YES |
NO |
NO |
|
JAPAN20 |
"J20" |
YES |
NO |
NO |
|
JAPAN21 |
"J21" |
YES |
NO |
NO |
|
JAPAN22 |
"J22" |
YES |
NO |
NO |
|
JAPAN23 |
"J23" |
YES |
NO |
NO |
|
JAPAN24 |
"J24" |
YES |
NO |
NO |
|
JAPAN25 |
"J25" |
YES |
NO |
NO |
|
JAPAN26 |
"J26" |
YES |
NO |
NO |
|
JAPAN27 |
"J27" |
YES |
NO |
NO |
|
JAPAN28 |
"J28" |
YES |
NO |
NO |
|
JAPAN29 |
"J29" |
YES |
NO |
NO |
|
JAPAN30 |
"J30" |
YES |
NO |
NO |
|
JAPAN31 |
"J31" |
YES |
NO |
NO |
|
JAPAN32 |
"J32" |
YES |
NO |
NO |
|
JAPAN33 |
"J33" |
YES |
NO |
NO |
|
JAPAN34 |
"J34" |
YES |
NO |
NO |
|
JAPAN35 |
"J35" |
YES |
NO |
NO |
|
JAPAN36 |
"J36" |
YES |
NO |
NO |
|
JAPAN37 |
"J37" |
YES |
NO |
NO |
|
JAPAN38 |
"J38" |
YES |
NO |
NO |
|
JAPAN39 |
"J39" |
YES |
NO |
NO |
|
JAPAN40 |
"J40" |
YES |
NO |
NO |
|
JAPAN41 |
"J41" |
YES |
NO |
NO |
|
JAPAN42 |
"J42" |
YES |
NO |
NO |
|
JAPAN43 |
"J43" |
YES |
NO |
NO |
|
JAPAN44 |
"J44" |
YES |
NO |
NO |
|
JAPAN45 |
"J45" |
YES |
NO |
NO |
|
JAPAN46 |
"J46" |
YES |
NO |
NO |
|
JAPAN47 |
"J47" |
YES |
NO |
NO |
|
JAPAN48 |
"J48" |
YES |
NO |
NO |
|
JAPAN49 |
"J49" |
YES |
NO |
NO |
|
JAPAN50 |
"J50" |
YES |
NO |
NO |
|
JAPAN51 |
"J51" |
YES |
NO |
NO |
|
JAPAN52 |
"J52" |
YES |
NO |
NO |
|
JAPAN53 |
"J53" |
YES |
NO |
NO |
|
JAPAN54 |
"J54" |
YES |
NO |
NO |
|
" |
"JO" |
YES |
NO |
YES |
|
" |
"KZ" |
YES |
NO |
YES |
|
" |
"KE" |
YES |
NO |
YES |
|
" |
"KP" |
YES |
NO |
NO |
|
" |
"KR" |
YES |
NO |
NO |
|
" |
" |
YES |
NO |
NO |
|
" |
"K3" |
YES |
NO |
NO |
|
" |
"KW" |
YES |
NO |
YES |
|
" |
" |
YES |
NO |
YES |
|
" |
"LB" |
YES |
NO |
YES |
|
" |
"LI" |
YES |
NO |
YES |
|
" |
"LT" |
YES |
NO |
YES |
|
" |
"LU" |
YES |
NO |
YES |
|
" |
"MO" |
YES |
YES |
YES |
|
" |
"MK" |
YES |
NO |
YES |
|
" |
"MY" |
YES |
NO |
NO |
|
" |
"MT" |
YES |
NO |
YES |
|
" |
"MX" |
YES |
YES |
YES |
|
" |
"MC" |
YES |
YES |
YES |
|
" |
"MA" |
YES |
NO |
YES |
|
" |
"NL" |
YES |
NO |
YES |
|
" |
"AN" |
YES |
NO |
YES |
|
" |
"NZ" |
YES |
NO |
YES |
|
" |
"NO" |
YES |
NO |
YES |
|
" |
" |
YES |
NO |
YES |
|
" |
"PK" |
YES |
NO |
YES |
|
" |
"PA" |
YES |
YES |
YES |
|
" |
"PE" |
YES |
NO |
YES |
|
" |
"PH" |
YES |
YES |
YES |
|
" |
"PL" |
YES |
NO |
YES |
|
" |
"PT" |
YES |
NO |
YES |
|
" |
"PR" |
YES |
YES |
YES |
|
" |
"QA" |
YES |
NO |
YES |
|
" |
"RO" |
YES |
NO |
YES |
|
" |
"RU" |
YES |
NO |
YES |
|
" |
"SA" |
YES |
NO |
YES |
|
" |
"CS" |
YES |
NO |
YES |
|
" |
"SG" |
YES |
YES |
YES |
|
" |
"SK" |
YES |
NO |
YES |
|
" |
"SI" |
YES |
NO |
YES |
|
" |
"ZA" |
YES |
NO |
YES |
|
" |
"ES" |
YES |
NO |
YES |
|
"SRILANKA" |
"LK" |
YES |
NO |
YES |
|
" |
"SE" |
YES |
NO |
YES |
|
" |
"CH" |
YES |
NO |
YES |
|
" |
"SY" |
YES |
NO |
YES |
|
" |
"TW" |
YES |
YES |
YES |
|
" |
"TH" |
YES |
NO |
YES |
|
"TRINIDAD & TOBAGO" |
TT |
YES |
NO |
YES |
|
" |
"TN" |
YES |
NO |
YES |
|
" |
"TR" |
YES |
NO |
YES |
|
" |
"UA" |
YES |
NO |
YES |
|
"UNITED
ARAB EMIRATES" |
"AE" |
YES |
NO |
YES |
|
" |
"GB" |
YES |
NO |
YES |
|
"UNITED
STATES" |
"US" |
YES |
YES |
YES |
|
"UNITED
STATES" |
"PS" |
YES |
YES |
YES |
|
" |
"UY" |
YES |
NO |
YES |
|
" |
"UZ" |
YES |
YES |
YES |
|
" |
"VE" |
YES |
NO |
YES |
|
"VIET |
"VN" |
YES |
NO |
YES |
|
" |
"YE" |
YES |
NO |
YES |
|
" |
"ZW" |
YES |
NO |
YES |
5.57 SINEMA E Site Survey: It is
not possible to capture 184,188 (
Site survey won't support
5.58 The current SINEMA E version, following devices will be using
“Alpha Networks wireless card with Atheros chipset“ country certification
instead of “siemens wireless card“ country certification.
·
All W786 types (RJ types: HW
revision 3 and higher; FO types: HW revision 4 and higher)
·
All W784 types and all
inherent client types
·
All W788 new hardware types
and all inherent client types with order number like “6GK57xx-xAA60-xAx0”
5.59 Load to SINEMA: Assigning
online device to project devices.
If
there are offered more devices you have to choose a device from the list with
the type and the firmware version which is corresponding to your device. At
some devices you find the HW release. Please have a look at HW release for the
online device and choose the corresponding device in the list of device to
assign.
If
the offered device contains the name like “scalance*-#1* “: There exist a
multiple devices with same firmware version and same type of devices. #
represents the count of such devices. This type convention is avoided by adding
significant part of the order number to name for new hard ware devices.
5.60 Information regarding country
certification for Scalance W devices.
Please
check the latest country certification list, which can be found here: http://www.siemens.com/simatic-net/ik-info
5.61 SINEMA E Site Survey:
Create User Defined Data Record
In the dialog “Create User Defined Data Record” the field “Wireless
Adapter name” is going to be filled with an adapter from the mixed data
records. The field “Mac Address” is then to be filled according the entry in
“the field “Wireless Adapter name”.
5.62 Using Remote Desktop for
operating SINEMA E
On some machines it may happen that SINEMA E will crash when it’s being
operated via Remote Desktop. In such cases there is no other solution than not
using Remote Desktop for operating SINEMA E.
5.63 Information regarding
Firmware Update feature
The devices in plant have to support “SNMP version 1”. “SNMP public
community” and “SNMP private community” will be used for authentication at the
devices. Sinema E needs write access to the devices. “SNMP public community”
corresponds to the “Read community
String” of the devices. “SNMP private community” corresponds to the “Read/Write
community String” of the devices.
In Firmware Update the functions of the 2 buttons is as follows:
- “Prepare Load”: The selected
Firmware is being transferred to the device by the TFTP-server.
- “Load and Reboot”: The device
is just being rebooted.
5.64 TIA – Totally Integrated
Automation
Using TIA under Windows Vista the
user Siemens TIA-engineer is not released for using SINEMA E.
5.65 Change of the deployment country
Please close all SINEMA E windows if you intend
to change the deployment country in the project properties.
5.66 Selection and alignment of antennas in the
modeling editor
The usability for antenna selection and
allignment has been improved with SINEMA E 2006 + SP4.
The new antenna-selection-dialog displays all
antennas from the catalog including their name, gain and characteristic.
When aligning (rotation and tilting) the
antenna in the modeling editor the respective antenna pattern (propagation
characteristic) will be displayed.
The horizontal and vertical antenna patterns
are particularly helpful when rotating and tilting directional antennas e.g.
ANT795-6DN.
In order to adjust the angle, click the
drop-down-menu in the „rotation“- or „z-axis angle“-field, a dialogbox with the
antenna pattern and a slider will be opened. Both the horizontal direction as
well as a red arrow at the antenna in the modeling editor will be displayed.
This arrow indicates the rotation in the
horizontal plane and does not change with alterations of z-axis angles.
Note:
The displayed antenna patterns (propagation
charateristic) are based on the antenna-catalog. The orientation of the
patterns in the catalog is mirrored with respect to the modeling editor
(simulation)! This has to be considered when alligning and simulating the
antenna.
Parameter "Rotation":
The red arrow at the access point in
the modeling editor points in the actual propagation direction. On the other
hand the antenna-pattern is mirrored.
Parameter "z-axis angle":
The antenna pattern in the z-axis is
similarily mirrored, i.e. the actual direction is reversed. As the modeling
editor is only a 2D display there is no corresponding red arrow for the tilting
angle (z-axis) in this case.